Texas Instruments prices $3.5 billion of investment grade notes
$500 million of 0.875% notes dueMay 15, 2013 $1.0 billion of floating rate notes dueMay 15, 2013 $1.0 billion of 1.375% notes dueMay 15, 2014 $1.0 billion of 2.375% notes dueMay 16, 2016
TI intends to use the net proceeds from the sale of the notes primarily to fund the merger with
Morgan Stanley &
The offering of the notes is made only by means of a prospectus, copies of which may be obtained from Morgan Stanley &
This news release does not constitute an offer to sell or a solicitation of an offer to buy any of the notes or any other securities, nor will there be any sale of the notes or any other securities in any state or jurisdiction in which such an offer, solicitation or sale is not permitted.
About
TXN-F
SOURCE
News Provided by Acquire Media